This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848K使用疑问

如下问题是在用到贵司83848k制作板子时产生的疑问,请指导一下

1
、当与83848k 对接端设置为10M全双工模式,83848为自协商模式,协商结果是10M半双工模式吗?

2
、当与83848k对接端设置为10M全双工模式83848为通过电阻把21,,22脚通过电阻下拉到地(目的是设置10M全双工),这种情况下83848k的工作模式是什么?

3
、如何通过寄存器把83848k强制设置为10M全双工?

4
、当83848k工作在10M半双工模式下,是否内部被环回了,不能和其余端口通信,如何通过寄存器去掉该换回

  • 1.对接端配置为10M 全双工模式的话,DP83848自动协商配置好,协商结果也是10M全双工。
    2. Pin21, 22 是Reserved和AVDD引脚。 如果您想设置10M全双工,通过引脚配置的话,需要将AN_EN=0,AN1=AN0=0
    3. 通过寄存器ANAR 04h bit6=1 来配置10M全双工。
    4. 配置为10M半双工不能通信吗?如何配置的?