This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB947-Q1使用疑问

调试947遇到无法点亮Deserializer端lvds问题。lvds 24位 1920*720 SPWG mapping,Twisted Pair.

调试发现0x0c寄存器值总为4,怀疑可能是fpdlink没连接成功的原因,请问可能是哪里的问题?cable和Deserializer端设备在其他机器上验证过是正常的。

0x0c寄存器 bit0 LINK detect status可以用了判断连接吧?开机后缺省是Twisted Pair,如不配置任何寄存器,应该也能反应Deserializer端的连接状态吧?


以下是当前主要寄存器值:

<3>reg00 = 0x18

<3>reg01 = 0x80

<3>reg03 = 0xda

<3>reg04 = 0x90

<3>reg05 = 0x00

<3>reg06 = 0x00

<3>reg07 = 0x42

<3>reg08 = 0x42

<3>reg0a = 0x00

<3>reg0b = 0x00

<3>reg0c = 0x04

<3>reg0d = 0x20

<3>reg0e = 0x00

<3>reg0f = 0x00

<3>reg10 = 0x00

<3>reg11 = 0x00

<3>reg12 = 0x00

<3>reg13 = 0x8e

<3>reg14 = 0x00

<3>reg15 = 0x01

<3>reg16 = 0xfe

<3>reg17 = 0x1e

<3>reg18 = 0x7f

<3>reg19 = 0x7f

<3>reg1a = 0x01

<3>reg1b = 0x00

<3>reg1c = 0x00

<3>reg1d = 0x00

<3>reg1e = 0x01

<3>reg1f = 0x00

<3>reg20 = 0x00

<3>reg26 = 0x00

<3>reg48 = 0x00

<3>reg49 = 0x00

<3>reg4b = 0x00

<3>reg4f = 0xc0

<3>reg50 = 0x16

<3>reg54 = 0x02

<3>reg55 = 0x00

<3>reg57 = 0x02

<3>reg5a = 0x0d

<3>reg5b = 0x21

<3>reg5c = 0x02

<3>reg5d = 0x06

<3>reg5e = 0x44

<3>reg5f = 0x27

<3>reg60 = 0x22

<3>reg61 = 0x02

<3>reg62 = 0x00

<3>reg64 = 0x10

<3>reg65 = 0x00

<3>reg66 = 0x00

<3>reg67 = 0x00

<3>reg70 = 0x00

<3>reg71 = 0x00

<3>reg72 = 0x00

<3>reg73 = 0x00

<3>reg74 = 0x00

<3>reg75 = 0x00

<3>reg76 = 0x00

<3>reg77 = 0x00

<3>reg78 = 0x00

<3>reg79 = 0x00

<3>reg7a = 0x00

<3>reg7b = 0x00

<3>reg7c = 0x00

<3>reg7d = 0x00

<3>regc2 = 0x80

<3>regc6 = 0x00

<3>regc7 = 0x00

<3>regc8 = 0xc0