This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用1.8V IO电压的FPGA 接收 LMH0341的数据,处理后通过LMH0340输出, 但这两个编解码芯片都是3.3V 的,
(1) 它们的控制信号我通过电平转换芯片连接吗?i2c控制pin SDA,SCK也可以通过通用的电平转换芯片连接吗?我看TI有专门的I2C信号电平转换芯片TCA9800,使用通用芯片可以吗
(2)LMH0341解码后的LVDS数据如何与1.8V IO的FPGA连接呢? 是交流耦合还是直流耦合? 同理FPGA输出的LVDS信号如何与 LMH0340连接呢?
(3)有1.8V 电压的 SDI 编解码芯片吗?
LMH0341的LVDS输出是800mV,你看一下FPGA1.8V的LVDS的摆幅是多少?如果可以匹配,就AC耦合就可以了