This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

sn74lvc8t245输出电流问题

这是芯片手册给出的单个IO输出电流相关参数

芯片VCCA侧采用3.3V供电,VCCB侧采用5V供电,如果VCCB方向从A到B,B侧每个IO输出,且同时输出,最大电流32mA。这样8个IO总共需要250mA电流

但是下面给出的IO最大才100mA,这样会不会有问题?

  • 是的,也就是说所有IO都工作的时候,最大不能超过100mA。 您刚才计算的那个是最大功耗,即静态电流+ 输出电流*8 约为256mA。 但受到这个100mA的限制,因此如果需要某个通道输出最大电流的话32mA的话,那么最多三个通道工作,其他几个通道就不能带载了。
  • 所有IO全部工作的时候,既需要满足整体电流不要超过100ma,也需要满足单个IO的电流不能超过要求。
x 出现错误。请重试或与管理员联系。