Other Parts Discussed in Thread: TMDS181
大家好,我想用一个USB接口的IIC适配器去配置TMDS181。
我看到TMDS181 EVM上用到适配器的是TP240141。现在我手里有TI的USB-TO-GPIO适配器,也是支持IIC的,这个适配器可以用来配置TMDS181吗?上位机的软件都是一样的吗?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMDS181
大家好,我想用一个USB接口的IIC适配器去配置TMDS181。
我看到TMDS181 EVM上用到适配器的是TP240141。现在我手里有TI的USB-TO-GPIO适配器,也是支持IIC的,这个适配器可以用来配置TMDS181吗?上位机的软件都是一样的吗?
谢谢!
你可以通过J5 input connector,使用自己的I2C软件写寄存器。3.3V的I2C
如果使用TI的就只能用240141了
USB-TO-GPIO适配器因为是通过USB接口和PC连接的,所以作为HID device 能够被PC自动识别,不需要额外的软件驱动。
如何通过I2C进行读写的话, USB to GPIO 产品主页上提供了GUI配置软件以及user's guide,可以参考下: