If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
the most speed of ISO1176 at 50 meters,is faster than 10Mbps?
The maximum bus length is limited by the transmission line losses and the signal jitter at a given data rate.A rule of thumb states that the product of the line length [m] times the data rate [bps] should be <10^7. Although
the standard recommends 10 Mbps with 10m cable , today’s fast interface circuits can operate at data rates of up to 40 Mbps.