This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913/933 的时钟问题

Other Parts Discussed in Thread: DS90UB933-Q1

hi,

913/933不使用外部晶振,使用Pixel Clock From Imager as Reference Clock模式的时候,当sensor的pixel clock没有输出的时候,913/933能I2C控制sensor吗?

  • 当没有pixel Clock的时候,913就没有像素时钟信号,也就无法正常工作,那么整个FPD link 也是不正确的,因此也就不能通过I2C 控制sensor。
  • 913/933有internal clock,不能工作吗?
  • 你好,
    DS上913/933可以工作在外部时钟和Pixel Clock From Imager as Reference Clock两种模式。
    第一种外部时钟模式下,DS上比较清晰的写了,在PCLK探测到之前,使用internal clock。
    但是Pixel Clock From Imager as Reference Clock这种模式下,也是先使用internal clock吗? 有internal clock 是不是I2C通信应该就是没问题的呢?

    DS:When PCLK signal edge is detected, and 0x03[1] = 0, the DS90UB933-Q1 switches from internal oscillator mode to an external PCLK. Upon removal of PCLK input, the device switches back into internal oscillator mode. In external oscillator mode, GPO2 and GPO3 on the serializer cannot act as the output of the input signal coming from GPIO2 or GPIO3 on the deserializer.