This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83849ID在低温条件下不能正常工作

Other Parts Discussed in Thread: DP83849ID

我现在使用DP83849ID,工作在RMII模式下,100M,光纤收发。硬件上,FX_EN管脚2.2k欧姆上拉,AN0管脚2.2k欧姆上拉。但在-31℃左右开始,收发开始不正常。经过修改16h寄存器(PCSR)之后,才可以工作在-40℃下工作。经过对比,按照目前的硬件配置16h寄存器中的数据与对16h寄存器写入的数据不同之处在于bit3和bit5。我想问一下bit5中Forces 100Mb/s Good Link 和Normal 100Mb/s operation都是什么意思,有什么区别。bit3中FEFI 模式是什么作用



  • Forces 100Mb/s Good Link 和Normal 100Mb/s operation 的区别在于,一种是通过自动协商成功的100Mbps 操作,一种是非自动协商的结果,通过配置使其工作在100Mbps 模式下称之为Force 100Mbps。
    16h的Bit3 和Bit4 为RESERVED, 为0. 您这里的FEFI指的是哪个寄存器的bit 3?
  • 1、我通过外部上下拉就已经对PHY工作在RMII进行了配置,难道是没有起作用吗?

    2、16h寄存器(PCSR),通过datasheet,bit5和bit3完全和温度没有关系,为什么我修改了他们之后,就可以在-40℃条件下正常工作了呢?