各位大佬好,我最近采用TUSB8041 做了一个USB3.0的hub, 一共采用四片8041, 分出来12个USB口,在测试的时候发现,最多只能识别3.0的设备6个,再增加的话系统能够识别,但是无法使用,通过观察总线上,set_configuration 的值为0, 而且不单单是影响hub,而是影响了整个 root hub,也就是我在同一个root hub下的其他端口接入新设备都无法使用。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用四片TUSB8041, 那么每片的TUSB8041都只能识别USB3.0的设备是吗?TUSB8041 的上行端口USB_DM_UP和USB_DP_UP有接吗?
你好,我的TUSB8041电路按照推荐电路设计的,接了USB2.0和USB3.0信号,但是,目前只有2.0能够正常使用,3.0没有响应,不清楚什么原因