由于项目需要,使用8路FPD3的Camera,设计中需要使用2片ds90ub964,因为需要6路Camera同步,所以第一片ub964使用内同步模式,同时把配置GPIO0为帧同步信号输出,连接到第二片ub964,第二片ub964使用外同步模式,同步信号为GPIO0,这样可以实现6路Camera同步吗?TI的参考设计TIDA-00455 中使用的4路Camera做的环视拼接是通过同步实现的吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
由于项目需要,使用8路FPD3的Camera,设计中需要使用2片ds90ub964,因为需要6路Camera同步,所以第一片ub964使用内同步模式,同时把配置GPIO0为帧同步信号输出,连接到第二片ub964,第二片ub964使用外同步模式,同步信号为GPIO0,这样可以实现6路Camera同步吗?TI的参考设计TIDA-00455 中使用的4路Camera做的环视拼接是通过同步实现的吗?
两种方法实现同步:
1)使用外部同一信号源作为Frame sync同时给两片DS90UB964。
2.使用DS90UB964内部产生的Frame sync信号,一片输出给另一片作为frame sync。
您好,請問你的問題有解決嗎?
我這邊目前也有項目需求,要實驗2片DS90UB964分別從兩路MIPI同時輸入camera影像,有點類似您的狀況。
簡單框架圖如下:
MIPI CSI 0 <----> TI DS90UB964(0) <----> TI DS90UB933 <----> FPD_PORT3 <----> camera
|
| Frame Sync
|
MIPI CSI 1 <----> TI DS90UB964(1) <----> TI DS90UB933 <----> FPD_PORT3 <----> camera
目前我這邊也是用第一片(0) 964輸出Frame sync訊號,給第二片964 (1) 接收,但目前問題在於,總是有一路的MIPI影像會有切成兩半的情形。
不知道方不方便分享如何initial register,或是碰到這情況如何debug的思路,或是initial table?
非常感謝