Other Parts Discussed in Thread: TLK10002
您好!
使用贵司TLK10002芯片,MCU通过MDIO读TLK10002,MDIO速率2MHz,现在可以一次正确读0x00~0x06、0x09~0x0D等寄存器的默认值。
一、目前读TLK10002有2个问题:
1 无法正确读0x07和0x08寄存器的默认值,0x07和0x08寄存器默认值分别是0xDC04和0x0001,MCU目前读TLK10002 0x07和0x08寄存器都是0。
2 无法正确写0x07和0x08寄存器,分别向0x07和0x08寄存器写入0x0E00和0x0F00,MCU再读TLK10002 0x07和0x08寄存器都是0。
二、
1 请问0x07和0x08寄存器默认值分别是0xDC04和0x0001?不是0x00?
2 读0x07和0x08有什么其他注意事项吗?
谢谢!