This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB Redriver和Switch芯片使用的一点疑问

Other Parts Discussed in Thread: TUSB211, TS3USB31

 

请问下,现需要用到TUSB211和TS3USB31这两款芯片对USB2.0高速信号进行调节,TS3USB31这款芯片的OE引脚,如图所示,使用的是继电器,OE接COM公共端,NC接GND,NO接3.3V,这样给High和Low,是否正确,是否这样会导致此款芯片有一定几率并不能正确的开关USB D+ D-信号?谢谢!

Layout部分如下图所示,发现TS3USB31芯片并不能如datasheet的Layout Example那样,D+ D-信号能较顺利Layout。

  • TS3USB31的OE可以直接接地,使得TS3USB31 使能。
    TS3USB31的 NC 不用连接,悬空即可。
    RLK_USB1 这款switch是什么型号?您这里提到COM ,NO, NC 应该都是这颗芯片的引脚。
  • RLY-USB1是一颗继电器来的。TS3USB31的NC是悬空的。OE给高电平的时候我是直接通过继电器切换到LDO的3.3V输出,这样会不会有问题?给低电平的时候是通过继电器切换到GND。