Other Parts Discussed in Thread: ISO1540, TCA9406
如上截图是摘至ISO1540的datasheet。SDA1和SCL1输出低电平最高会有800mV。我们实测了有850mV。这样对于3.3V的EEPROM和3.3V的MCU来讲,低电平太高。根本就不能识别为0。不知道其他使用这颗料的工程师是怎么处理这个问题的?TI官方会不会有这种情况的应对措施。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
收到,非常感谢。确定不能只是使用一颗ISO1540来做3.3V系统的隔离。那我再想办法增加其他器件。
上图是PCA9406的参数介绍,是不是也说明当低电平输入为0.8V的时候,对应输出是大于0.8V的。也就是说,就算ISO1540+PCA9406也是不可行的。