Other Parts Discussed in Thread: PCA9555
您好:
关于PCA9555使用有几个问题,请帮忙确认一下。
1、想把电源LTC3789的PGOOD引脚连接到PCA9555上,目前LTC3789电源的PGOOD引脚上拉到INTVCC,而INTVCC的最大电压可以到5.8V,而PCA9555推荐的GPIO电压范围是2.3V~5.5V,在6.1 Absolute Maximum Ratings中,GPIO的最大输入电压是6V,请问直接把LTC3789的PGOOD引脚连接到PCA9555的GPIO上,有没有问题?
2、PCA9555手册说上电默认状态时输入引脚,并且内部有100K上拉到VDD,请问下此时默认状态下测量PCA9555的GPIO是不是应该是与VDD一样的高电平?另外此时GPIO的驱动能力是怎样,是否可以直接驱动MOS管(开启电压在1.5V)?