This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
利用TXB0108 实现自动双向数据的电平转换,VCCA=3.3v,vccb=5v ,可以实现吗?如果能够实现可以给出参考电路图吗?谢谢啦!
可以实现3.3V到5V的电平转换,您具体是什么应用? 因为它能够支持的最大data rate为100Mbps,所以要看是否支持您的应用?
另外,TXB010x或TXS010x的DC 驱动能力很弱,如果您的应用需要驱动能力比较强的话,建议使用带方向控制位的SN74xx系列的电平转换。