This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01281: 在 工业领域的通讯模块中,使用ISO1050有哪些好处?

Other Parts Discussed in Thread: ISO1050

在的低成本、高效率的工业领域(例如:UPS和储能系统)通信模块中,使用ISO1050(隔离5V CAN收发器)有可以带来哪些好处?

TIDA-01281 是TI的一个参考设计,它介绍了如何开发应用在工业领域中(例如:UPS和储能板)的低成本、高效率的RS-485, I2C和CAN通信模块。ISO1050 是一个电气隔离CAN收发器,符合 ISO11898-2 标准,并且隔离电压高达5000VRMS。 它的信令速率高达1Mbps,内置总线故障保护从-27V至40V。在TIDA-01281中,ISO1050 的使用实现了CAN的隔离通讯,以此来给外接的CAN控制器提供系统状态信息。

关于这个主题更多的信息, 请参考User Guide for TIDA-01281 的第2章节 " Communication in Power Supplies " 。你也可以从TIDA-01281文件夹中,下载更多的参考设计文件 (BOM, 原理图, Gerber) 。