This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB940 Pattern Generator问题

嗨,TI,

我司目前采用947和940的连接方案,940目前想用 Pattern Generator先行调试,我按照snla132c.pdf 第4.3 Custom Display Configuration进行配置,已经获得clk输出,但似乎不对,而且,我想知道940 mipi_csi输出数据的传输格式是什么?bt656或者其他?0x64是用于设置输出数据格式的,但是我找不到数据的传输格式在哪里设置。

  • MIPI_CSI的输出格式可以是RGB888,可以是RAW data,也可以是YUV, 在UB940的datasheet Table 10给出了具体配置:

    另外,pattern generation已经获得CLK输出,是哪里不对呢?

  • Kailyn Chen,

    你好,非常感谢你的解答。是这样的,用示波器测量clk只有大概18k左右,其次,Table10 是指数据格式,那数据的传输格式是什么呢?bt656是指传输格式之类的

  • YUV420就是YCbCr4:2:0 的传输格式,而BT656 指的是8 bit YCbCr 4:2:2格式 ,并且是内嵌HSYNC, VSYNC 信号。