This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ds90ub940 Pattern Generator 测试

Hi, Ti,我目前进行DS90UB940  Pattern Generator的测试,往ds90ub940寄存器写入如下值:0x65=0x04,0x64=0x35,然后示波器在csi0_clk可以测到62Mhz左右的频率,但是csi0_d0--csi0_d3却无法测到任何数据,Pattern Generator是否还需要其他的配置?

期待解答。

祝 好

  • 您好,
    链接:www.ti.com/.../snla132c.pdf 15页第4章节有配置示例,请参考下。
  • 你好。我按照snla132c.pdf第4章节进行配置,0x64(PGCTL)这个寄存器配置为0x31,按照手册应该是红色,可是我看到的却是绿色,而且有滚动条纹出现,如果配置成自定义颜色(0x64=0xe1,PGRS,PGGS,PGBS),也大都是绿色为主

  • 您好,
    寄存器0x65(PGCFG)的0和1bit配置的是什么,PGCTL的7:4bit在Auto-Scrolling Mode下无效。
  • 你好,0x65(PGCFG)写入0x04,所以,并没有使能Auto-Scrolling Mode。另外,根据imx6q MIPI_CSI.ERR1这个寄存器报错的信息来,应该是CRC校验出错,正常情况下MIPI_CSI.ERR1这个寄存器的值应该为0x00000000,但是现在确实0x01001000(对应的位是bit[24]和bit[12]),

    我找到解决方法如下:

    现在想通过第一个方法来尝试解决,该如何配置940的输出timing?

  • Amy Luo,

    您好,我在940的手册看到,看到如下描述,那请问我如果想要1920x720p60,PCLK=111.86MHZ,4 MIPI lanes, reg0x6c和reg0x6d该如何配置?

      940手册关于csi Indirect Register只介绍了下面这几个,