This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1294 is an SPI communication interface, how to design to use What about UART communication? Looking forward to replyingADS1294 is an SPI communication interface, how to design to use What about UART communication? Looking forward to replying

Other Parts Discussed in Thread: ADS1294

ADS1294 is an SPI communication interface, how to design to use
What about UART communication? Looking forward to replying

  • Hi chaoyun,

    It is recommended that you add a SPI to UART integrated chip or single-chip controller to realize it.
    Hope that can help you.

    Best Regards,
    Amy
  • dear ti:

    Because the main control system mounted ads1294 communication adopts uart serial communication which is the most convenient and the fastest debugging.So I would like to ask how can ads1294 communicate directly with serial port?At present, we have the development board of ads1294. How can we achieve serial port communication on the hardware and software?

    br