This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822以太网通讯信号完整性问题。



想测试一下DP83822以太网通讯的信号完整性,看到规格书里面提到了一个LOOPBACK模式,想问下这种模式是不是就是针对以太网信号测试的模式,怎么用?

测试100M以太网信号好不好,如何去评价?

  • loopback功能是DP83822的自环模模式,测试内部各个模块功能是否正常的一种检测方式。
    测100M网络信号好不好,看网络连接情况的话,可以通过LED 去判断。
  • 使用External Loopback 回环测试(需要手动把 网口的 1、3脚短接;2、6脚短接),使用以太网驱动模块发送一帧数据,受到的数据和发送的数据相等,就可以保证MAC到PHY,PHY到网口的硬件电路是ok的? 有无更简单的方法,我只验证 硬件电路的正常与否。