我现在需要实现1.2V I2C到1.8V I2C的转换,是否可以用PCA9306这颗料?
我看PCA9306规格书里面还写到En脚需要比VREF1和VREF2大1V才行,此时,如果我需要常使能EN脚的话,再接1.8V是不是就不合适了,
那么请问下此时EN脚、200K电阻、VREF2该如何接合适?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我现在需要实现1.2V I2C到1.8V I2C的转换,是否可以用PCA9306这颗料?
我看PCA9306规格书里面还写到En脚需要比VREF1和VREF2大1V才行,此时,如果我需要常使能EN脚的话,再接1.8V是不是就不合适了,
那么请问下此时EN脚、200K电阻、VREF2该如何接合适?
Vref1=1.2V的话, EN和VREF2 两个引脚可一起通过200Kohm电阻上拉到1.8V , 是可以进行电平转换的。
因为Vref2 和EN的电压最小值为Vref1+0.6V。 在datasheet 中Recommended electrical charactertistcs中也有给出解释:
To support translation, VREF1 supports 1.2 V to VREF2 - 0.6 V. VREF2 must be between VREF1 + 0.6 V to 5.5 V.
上面的红框内的EN是说EN信号要≥1+SCL吧,要是这样的话,那我SCL=1.2V时,EN脚=1.8V就没法满足条件了!
但是我看你回复的是En信号≥1V或者SCL。我不知道那个理解的对啊
谢谢