This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FPD-link serdes UH941A 的 HDCP 认证失败问题

UH941A 和 UH948A 配套使用,941初始状态HDCP寄存器配置如下:

reg 0xc2 = 0x80

reg 0xc3 = 0x00

reg 0xc4 = 0x68

 然后使能HDCP 认证和加密

reg 0xc2  = 0x90

reg 0xc3 = 0x01

发现与UH948A相连的屏幕蓝屏了,寄存器0xc4查看状态一直是0x6a, bit0 - AUTHED 一直为0.

同样的过程,把UH941A换成UH949A,HDCP就一切正常没问题,使能HDCP后,屏幕正常显示,寄存器0xc4查看状态一直是0x69,bit0 - AUTHED 一直为1. 把电缆插到使用UB948的屏幕后才蓝屏,

求教高手这UH941A 的HDCP是出什么问题了么?