This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108EPW 接口产生震荡

应用环境,并口打印机5V转3.3V

应用电路

D0-D7是并口,A测接STM32单片机配置为输入,无上下拉

D0-D7并口输入信号接的驱动芯片是SN74LVC4245

现象:信号线上会产生震荡,频率在34MHZ、8mhz等没有规律,34MHZ较多。

红框处应当是低电平的,此时D0-D7都是低电平,且都会有类似波形