This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LMX2581的手册上要求NO_FCAL控制字为0时,才能开始频率校准,当用到输出分频器时,又必须将0_dly控制字设为1,这就启用了zero delay模式,但是该模式下要求将NO_FCAL设为1,这应该怎么办??
那就是说我在0_delay模式下,需要改变频率,频率进行校准时,吧NO_FCAL设置为1就行吧。
还有一个问题,我用100MHz晶振做参考时钟,然后倍频为200MHz,phase detecor的频率为200MHz,VCO_DIV设为0,2分频输出,其中PLL_N设置为15,integer模式,VCO的频率为3000MHz,但在0_dealy模式时,N不能整除VCO_DIV,会降低phase detector 的频率,这时phase detector 的频率是多少?
手册中Program the PLL_N value with PLL_N* / VCO_DIV, where PLL_N* is the original value. 这个PLL_N*是original value,在我这里到底指的是多少?