This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lmk05318的lol*



在接入外部xo后,apll1不就应该自动频率锁定吗,接入参考后led灯显示的lopl、lofl都表示dpll的相位和频率都锁住了。当我把led灯显示为(PLL1 lock detected(lol* )时就一直不亮,问题出在哪里呢?

还有,追踪参考输入成功后,是需要手动分频调整成与参考一致的频率输出,还是outputx直接可以自动输出与参考频率一致的波形?

  • 您好,

    在我的应用场景中需要用到一种隔离器件,输入信号的电压幅值为12-24V,输入电流小于20mA,输入频率约20Hz。我要将这个信号转换成3.3V的电压信号。但是必须要使输出信号相对于输入信号的延迟在1us以内,最好在500ns之内,并且不能改变输入信号的占空比。

    我原来使用的的方案是高速光耦,其输入的延时可以满足要求(< 1us),但是输出延时为3us,这就改变了输入信号的占空比,不满足需求。

    请问TI是否能满足我需求的转换芯片提供?

  • 我们的数字隔离器ISO7xx系列的传输延迟控制在405nS之内,所以传输延迟能满足您的要求。

    但是电压范围最大5.5V,不能满足12~24V的范围。