This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问CAN收发器SN65HVD230和234之间有什么区别呢?

看功能似乎基本一样?

  • 首先操作温度范围不一致,230的温度范围为-40~85度,而234的操作温度范围更广一些,为-40~125度
    其次总线电压范围也一样,230的CANH或CANL的电压范围为-4~16V,而234的CANH或CANL的电压范围为-36V~36V。
    另外,234 还兼容GIFT/ICT Compliant。
    以上是二者的主要区别。