我们现在计划使用AWR1642实现我们的传感器方案,传感器需要将数据传输出来,计划采用LVDS转RGB的方式,由具备RGB接口的ARM接收并显示出来。
AWR1642是LVDS接口,但我们查看TI的LVDS转RGB的芯片,例如SN65LVDS306,都是标明subLVDS的,请问SN65LVDS306能不能和AWR1642直接相连?有没有类似的参考手册,或者应用案例供我们参考?如果LVDS不能用subLVDS的接口转换芯片,有没有芯片帮忙推荐一下,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们现在计划使用AWR1642实现我们的传感器方案,传感器需要将数据传输出来,计划采用LVDS转RGB的方式,由具备RGB接口的ARM接收并显示出来。
AWR1642是LVDS接口,但我们查看TI的LVDS转RGB的芯片,例如SN65LVDS306,都是标明subLVDS的,请问SN65LVDS306能不能和AWR1642直接相连?有没有类似的参考手册,或者应用案例供我们参考?如果LVDS不能用subLVDS的接口转换芯片,有没有芯片帮忙推荐一下,谢谢!
subLVDS和LVDS的电压swing还是有区别的。所以LVDS和subLVDS是不能直接相连的。
LVDS转RGB的话,您可以参考DS90CF386:
谢谢你!再向您请教两个问题:
一,我们觉得DS92LV16挺好的,只是它既有解串器也有串行器,有没有只有两个或者稍多点也行的解串器的,串行器我们用不上。
二,我们的外设,它的LVDS是12bit一帧,不是16个bit一帧,解串器可以正常工作吗?它是不是可以把12bit合起来,作为一个数据,以DS92LV16来说,其上4bit就空为0了呢?谢谢了!
你好,我是一个新手,也用到AWR1642把二次开发,我想向您请教如果如果通过LVDS把数据传输给FPGA,相关的配置和lvds接口数据在AWR1642的用户手册里吗?直接AWR1642boost评估板的60-pin HD connection 接口输出信号,然后再转成自己需要的格式可以吗?
谢谢。