我们现在用到了器件,其输出LVDS接口,一个帧12bit数据,有bitclock和frameclock,也就是说,frameclock是bitclock的6倍。(由于帖子不能附图,无法把时序贴出来),现在想将LVDS转成并口,用ARM读取该数据,不知该选择什么样的器件?
之前有TI的工程师建议我们采用DS90CF386,实现LVDS到RGB的转换,我们在读DS90CF386的时候发现,由于它是实现LVDS转RGB,所以一个frame内只有7个bit的数据。现在的问题是,我们一个帧12bit数据,能否用该器件进行串并转换呢?
另外,TI的工程师推荐我们使用DS92LV18,对于这样的器件,我们没有看到它有bitclock的输入管脚,是否意味着它无法实现我们的要求?
现在的问题是,对于一帧12bit的LVDS接口,如果要把它转换为并口输出,选择哪一款芯片比较合适?谢谢!