Other Parts Discussed in Thread: TCA9539
用USB到SMBus的桥接芯片CP2112 做TCA9539的主设备,在写从设备地址时,TCA9539不应答。
TCA9539 VCC接3.3V ,INT和reset都不使用,10K上拉到3.3V,A0A1接地,写E8无响应。
折腾了很久,实在找不到为什么?
还请帮忙解答,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TCA9539
用USB到SMBus的桥接芯片CP2112 做TCA9539的主设备,在写从设备地址时,TCA9539不应答。
TCA9539 VCC接3.3V ,INT和reset都不使用,10K上拉到3.3V,A0A1接地,写E8无响应。
折腾了很久,实在找不到为什么?
还请帮忙解答,谢谢!
是1k上拉
主机这边就是I2C接口 ,TCA9539与另一个I2C设备一起共用I2C总线,另外的设备可以正常读到地址
9539跟另外的设备也不存在地址冲突问题
断开另一个设备TCA9539也不工作
我测了I2C的波形,100K频率,是满足时序要求的
之前有看到过别人说TCA9539 R/W为1时设备是没有应答的,我也试了确实还是不行
确实是SMBus总线,芯片写的SMBus协议频率最高支持255khz ,你说的高于100kHz就收不到ACK了是指TCA5939默认工作模式是fast mode的400kHz吗?这个要怎么验证 ,那主控支持不了400k就没法工作了么?
另外我的R/W位不管0还是1时候都收不到ACK应答
您好!发现之前的结论只是偶然识别到了 ,多几次后就发现依然是大概率识别不到TCA9529
求助可还有什么别的思路