TI的工程师,你们好!
我们使用DS90UB954 DS90UB953进行图像采集,发现通过954配置sensor后,954的MIPI接口发现数据len是有信号了,但是时钟len却没有信号,我们配置了0x33这个寄存器为0x23的值,并且读取了954寄存器的值,发现该0x33寄存器的值确实为0x23,但是时钟len依然没有信号,请问这是什么原因?还有哪里需要注意的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI的工程师,你们好!
我们使用DS90UB954 DS90UB953进行图像采集,发现通过954配置sensor后,954的MIPI接口发现数据len是有信号了,但是时钟len却没有信号,我们配置了0x33这个寄存器为0x23的值,并且读取了954寄存器的值,发现该0x33寄存器的值确实为0x23,但是时钟len依然没有信号,请问这是什么原因?还有哪里需要注意的?
lock输出为高电平,数据lane有信号(幅值为200mv和1.2V方波),时钟lane为200mv附近正弦波,但是摆幅只有不到50mv,不知道是否正常,主控接收平台捕捉不到camera数据