This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB933能否支持1080p 30帧 并口信号?

求教:

1、车载摄像头 1080P30帧信号 可以用哪些编码器, DS90UB913是不是只能做720p 30帧的?

2、解码器可以接所有型号的编码器信号么?

3、DS90UB914接入DS90UB933信号可以解码吗?能够支持到1080p30帧的信号解码么?

4.  DS90UB933能否支持1080p 30帧  并口信号?

  • 1. DS90UB913A能够支持的像素时钟频率范围最大为100Mhz,而1080p@60fps需要的pixel clock 为148.5Mhz,那么1080p 30的像素时钟为74.25Mhz,所以是支持的。
    2. 编解码器件 不是所有都能搭配使用的,要看实际应用。
    3. 914A可以和933 搭配使用,914A像素时钟最大也是100Mhz.
    4. 同样,933 支持像素时钟最大也是100Mhz,而1080p 30fps的像素时钟需要74.25MHz,所以也是支持的。