This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD82DR的AB电平异常



请教下,SN65HVD82DR使用中有点疑问,简单电路如下,5V供电;但是在给通过RS485给产品升级时,速率115200,子模块接受到后会发送一个信号。当主模块中的数据包中出现连续较多的F时,子模块返回的信号幅值就会异常,如下图A-B的幅值在-440mV--4.8V,如果连续F较少时,A-B的幅值是-4.8V--4.8V之间。想了解下有可能是什么原因造成的。

目前主模块与子模块间的RS485电路架构一样。