This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4020BI-Q1操作條件問題

Other Parts Discussed in Thread: TUSB4020BI-Q1

Hi All,

在TUSB4020BI-Q1的datasheet中可以找到,最高的junction為105度。在AEC-Q100中,最低的ambient溫度為Grade3的-40~85度,這樣TUSB4020BI-Q1大約還有20度的溫升範圍。因為Hub IC(TUSB4020BI-Q1)溫度的考量,有幾個如以下的應用問題要麻煩各位幫忙確認,感謝。

  1. TUSB4020BI-Q1有支援high-speed, full-speed, low-speed種模式。在datasheet中,可以找到有提供high-speed模式下一個port與兩個port工作下分別所需的電流。但是沒有full-speed, low-speed的數據,可以麻煩各位幫忙提供嗎?
  2. 因為有發現大部分Hub IC對於不同的傳輸速度,都會有不同的功耗。另外,目前看到需要最大功耗的是在2個port都運行在high-speed的時候,那當資料傳輸結束時,所需的電流是否就降回到Suspend的這個條件呢?
  3. 在USB2.0的規範中,最高的操作速度是在high-speed模式,傳輸速度大約為60MB/S。在車上的USB應用上,會是跟車載的影音系統做連線,可能會傳輸音樂或是影像檔案。以比較大的電影檔案來說,假如為1.45GB,以60MB/S的速度傳輸,這樣大約只有30秒。而TUSB4020BI-Q1是不是就只會有30秒的時間會有較大的電流需求,而傳輸結束就會降低工作電流嗎?
  4. 在規格書中可以看到操作溫度為-40~105,當junction溫度操作超過105是否就會造成IC損壞呢?當溫度太高但又沒操過105時,對於IC會造成什麼影響呢?IC的特性與行為會有改變嗎?
  5. 接續前面的問題,我們是否可以設計一個溫度檢測機制。當檢測操過一定溫度時,可以減少IC的效能,例如:降低資料傳輸的速度,以減少功耗呢?有類似的設計範例可以提供嗎?