This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tfp401使用

Other Parts Discussed in Thread: TFP401, DS16EV5110, TFP410

你好,现在有一个HDMI接口的摄像头,连接到一个均衡器DS16EV5110,在连接到tfp401的输入,之后送给fpga,怎么判断fpga接受到信号是否有问题?

在tfp401没有找到RGB的时序图,这个怎么判断好坏?

  • 时序的话可以参考 Figure 5 Data Setup and Hold Times to Rising and Falling Edges of ODCK 以及7.7 部分的AC characteristics。
    先用示波器测量下ODCK, data, HSYNC, VSYNC这几个信号,对比Figure5 ,从而判断TFP401输出是否正常。
    www.ti.com/.../tfp401.pdf
  • 还有,fpga接到rgb信号,直接环回给tfp410,再送给显示。请问这个有什么特殊要求,网上查到说是要求输出hdmi端口通过IIC读取显示器内部的eeprom内容,这个IIC是否是必须要的操作?
  • 为什么tfp401手册写着最高1080@60Hz,但是换成1080@30Hz就不行了?
  • TFP410可以不使用I2C 也是能正常工作的。所以通过I2C去读取EEPROM的值不是必要的。
    所以FGPA 接到RGB信号环回给TFP410 接显示我认为是没问题的。
  • TFP410可以不使用I2C 也是能正常工作的。所以通过I2C去读取EEPROM的值不是必要的。
    所以FGPA 接到RGB信号环回给TFP410 接显示我认为是没问题的。
  • 1080@30Hz 也是能支持的,换成30Hz 之后是哪里出问题了?
  • 这个30HZ有误会。是这样的,我们将服务器上HDMI端口设置为1080@60hz输出,连接我们板卡,通过板卡处理之后送给显示器可以输出,这个正常显示;但是将摄像头,HDMI输出1080@60HZ,连接板卡,就没有输出。这两种HDMI不一样吗?不知道tfp401和tfp410对于这两种视频源有什么限制没有?