This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
第一次使用933、934,不是很熟悉,有几个问题咨询。
目前在做一款产品,大致是 FPGA->933->934->usb;
FPGA传给933是8bit data和行场信号及pclk;
934输出的也是8bit data和行场信号及pclk;
目前疑问是:
1、933和934的VDDIO是否需要一致电压还是可以一个1.8V一个3.3V?
2、933的VDDIO为1.8V,是否需要对933 0x01寄存器bit4置0,默认值是1?
3、如果需要对933的寄存器修改,是由FPGA使用i2c对933寄存器进行读写,还是由USB 使用i2c对934寄存器读写(因为网上看到可以通过914配置913,具体怎么实现不是很清楚,不知道933/934是否也可以)?
4、933、934的i2c设备地址在硬件电路上有IDX引脚控制?如果IDX接地,933的设备地址是0xB0,934是0x60?