This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04808 PLL2锁定输出

Other Parts Discussed in Thread: LMK04808

用LMK04808 PLL2 输入100M的信号, 倍频到3000M, 再分频到200M . SYNC控制。 发了PCB板,用单片机控制。 现在锁定到200M输出。但是 如果将EN_PLL2_XTAL=0, 断开100M的输入, 输出也有204M.  问题是:这是的输入从哪儿来的?怎么还有输出?

  • 您好,
    EN_PLL2_XTAL bit 不是用来断开PLL2 参考输入的,在数据手册73页 8.6.3.4.9 EN_PLL2_XTAL有说明:If an external crystal is being used to implement a discrete VCXO, the internal feedback amplifier must be enabled with this bit in order to complete the oscillator circuit.
    如果使用外部的晶振实现离散VCXO,则必须使用该位使能内部反馈放大器,以完成振荡器电路。