This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB927/928方案偶现雪花点问题



请教一个问题,背景描述如下:

1、采用DS90UB927/928方案,概率发生开机后界面出现零星的雪花点,且不消失。

2、发生该问题时,量测928的LOCK、PASS信号管脚,未出现任何跌落,ERROR寄存器未发现错误。

3、对927/928分别进行内部时钟和外部时钟的BIST检测,也未发现异常,ERROR寄存器未发现错误。

4、对927/928分别进行pattern模式检测,正常。

5、发生该问题时,对927/928进行硬复位或软复位,均可恢复正常。

6、927/928的VDD、VDDIO、PDB上电时序正常。

有以下几个疑问,烦请大佬们解答下:

1、该雪花点问题,可以通过对927/928进行硬复位或软复位来恢复正常,看起来问题可以得到解决,但无法解释根因?

2、如果是LVDS的走线质量问题,或是时钟抖动问题,不太可能通过对927/928进行复位就能解决?

2、927和928之间的上电时序有要求吗?初始化先后有要求吗?