This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI大大们好,
我们使用913+914方案,STP模式,Sensor是IMX323,Sensor晶振37.125MHz,通讯已正常,STP线已做屏蔽+双绞,主板端为2.54间距wafer连接器,Sensor端是1.0间距Wafer连接器,静止放置长时间运行正常。
但拿起晃动中间线缆或者触碰PCB,就容易数据丢失,图像卡住,VIN丢失。
开始觉得是接触不好,所以将两端的端子都使用UV胶固定,保证晃动时端子不晃动,测试效果稍微好一些,但仍然会发生,目前一直没有彻底的解决。
我们在软件上检测914的0x1C状态寄存器,以应对这种通讯异常,重新启动主控端的Sensor数据接收,但这终究还是没有彻底解决,用户体验很差。
所以发帖求助一下,STP模式下,我们应该怎样接线会更可靠,两边端子通常使用什么的连接器,PCB上应该如何处理能更抗干扰一些。
恳请赐教,谢谢。
附件 913 914的原理图
Hi Kailyn,
感谢回复。
我查看了snla229.pdf文档,关于ReturnLoss
Return Loss is the loss of the signal power resulting from a discontinuity in the characteristic impedance of the transmission line, and is most commonly encountered at the interface of one portion of the transmission line and another – such as the connector to a cable or board.
所以看样子貌似主板和线之间的连接很关键,看了官方的好多资料,包括开发板都是同轴电缆的连接方式,最佳阻抗推荐为50Ω,由于产品外观和体积上的限制,目前我们采用的传统的2.54 wafer连接器(主板端),1.0 wafer连接器(Sensor端),请教下其他客户有没有使用STP模式的,使用了何种连接器?STP模式推荐用什么连接器?STP线缆的阻抗也为50Ω吗?
感谢。