This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108如果两端都供电3.3V,那么A端信号电平是3.3V,B端输入电平是5V的信号,可以正常通信吗?



TXS0108如果两端都供电3.3V,A端输入输出信号电平是3.3V,而B端被输入5V电平的信号,可以正常通信吗?

  • 您好,

    不能保证可以正常通信。A和B信号口可以输入的高电平范围是VCCI,即A信号口可以输入的最高电平的VCCA,B信号口可以输入的最高电平的VCCB。因此若VCCB是3.3V,那么B信号口可以输入的最大电压是3.3V。