This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB964的诊断问题



你好:

1、有没有什么办法能够诊断出UB964芯片是否故障,是否还在工作,比如可以通过读什么寄存器的值进行判断?

2、如果发现芯片有故障,通过什么办法可以对芯片进行复位操作;多谢!

  • 1. 您先按照datasheet中P48的Pattern Generator code example 看下显示器是否能显示colorbar?
    2. 对964 进行复位可以通过PDB这个引脚来实现,PDB =L 的时候964 进入shut down状态,PDB=H的时候enable 964.
    所以如果需要对其进行reset,可以将PDB拉低。然后在拉高进行一个复位动作。