Other Parts Discussed in Thread: DS90UB941AS-Q1
4路1百万摄像头合成全景后,DSI输出给到另外一个控制器CSI输入。
SER2用UB941,DES2用UB940,是否可以满足需求。另外如果DES2现在固定为了UB954,请问有什么解决方案
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS90UB941AS-Q1
4路1百万摄像头合成全景后,DSI输出给到另外一个控制器CSI输入。
SER2用UB941,DES2用UB940,是否可以满足需求。另外如果DES2现在固定为了UB954,请问有什么解决方案
您的意思是使用SER2采用941, DES2 使用954, 无法对接成功是吗?
还是由于954 是双路的,想将SER2和SER4的输出直接接954 ,然后954 对两路的数据进行各自解码输出CSI数据?
是的,我想问,ser2用941能不能与des2的954成功对接。如果不能,ser2这边有什么方案能实现dsi转fpdlinkiii并能与des2的954对接
Dear Kailyn Chen,
这个问题有解决吗后面,我们也遇到同样的问题,954定了,前面能不能加转接芯片?