This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB947和DS90UB948问题



TI工程师

      你好

   我司现在有个车厂前装项目有用到DS90UB947+DS90UB948来传输视频和触摸信号。屏的分辨率为1920X720,双路LVDS输入。如果通过I2C配制947寄存器为双路LVDS输入,双路FPDLINK输出,948寄存器为双路LFPDLINK输入,双路LVDS。显示屏无输出,LOCK信号电平跳变。如果通过I2C配制947,948为其它配制,显示屏有输出,但是显示效果很差,向那种奇偶场反的感觉。请问下,947和948只通过电阻来设置MODE_SEL0,MODE_SEL1和其他设置脚就能正常按我要求的工作还是一定需要通过I2C去配制,能发下满足我要求的I2C初始化的代码吗?

  • 通过寄存器配置,或者通过引脚配置都是一样的。所以947 或948 都通过IC 配置,是问题的。
    所以问题的原因不在这里。
    显示屏无输出的话,那么有通过示波器测量下948 的输出波形吗?是否正常?