This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04828 配合TRF3765 温度升高不输出

Other Parts Discussed in Thread: LMK04828, TRF3765, ADC12J4000

你好

     我们想用TRF3765分频。用LMK04828 输出频率。按手册设计,在室温中开始上电正常。,工作2分钟左右就不输出了。开空调在上电就可以一直工作,这样的问题应该查找什么方面的,之前做个单路的,使用的是一路ADC12J4000的,这次集成了2路,用了2片ADC12J4000。请指教如何解决。谢谢。

  • 您好,

    应该是芯片散热没有做好,LMK04828的thermal PAD 应该与PCB地多打孔大面积连接进行散热,可参考数据手册11.1 Current Consumption/ Power Dissipation Calculations芯片电流计算芯片发热功率,判断芯片结点温度是否超过125℃。
  • 你好

         散热没有做好这个有可能,但问题是芯片工作大概不到2分钟,看着正常的波形就一点一点的变没有了。空调也不是直直对着板子吹,离开有1米多距离。只要吹着。工作起来就没有什么问题。即使说温升应该不会在不到2分钟的时间升到125度吧,再就是假如升到125度是不是芯片就保护了。除了散热我还需有其他需要注意的吗。谢谢。

  • 几分钟到达125℃是与散热、外部坏境温度有很大关系的,如果散热特别不好几秒钟就达到了。建议测量一下Icc电流,根据室温计算一下温升,根据数据计算判断一下芯片结点温度是否超过125℃,以确定芯片不工作的原因。