This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问关于DS90UB925 通过LVDS连接 DS90UB928,如何控制928的GPIO状态



请教TI工程师,如题

 车载中控主机端为DS90UB927,通过LVDS连接到 显示屏端的DS90UB928,工作正常。现在我们自己做了一个主机替代原车主机,MCU+DS90UB925,现在通过LVDS传输,视频信号显示正常,说明LVDS通路正常,但是原显示屏端的DS90UB928,PIN14 GPIO0这个脚状态不对,导致背光不能打开,请问,在925主机这一端,如何实现控制928的GPIO?(显示屏端的DS90UB928不能做任何改动)

     因为对这个芯片不熟悉,麻烦详细说明如何实现的,感谢!

  • 您好,

    您可以参考下这个文档:www.ti.com.cn/.../snla234.pdf
  • Amy Luo   你好

       感谢回复

       但是我看了文档那个还不太明白,有几个问题请教一下:

    1. 925端的GPIO0和928端的GPIO0 有没有对应关系?就是在925端通过硬件货I2C配置了GPIO0的状态,是否能在928端的GPIO0输出同样的状态?还是说两边的GPIO完全是独立不相关的?

    2. 我在925端可以通过外部I2C工具读取925的寄存器配置,也可以修改配置,但是,没法读取或修改928端的寄存器配置,这个操作需要如何实现(目前925和928的LVDS是ok的,因为视频信号传送正常)

                                                                   谢谢了