我的相机采用AR0144,它的内部集成TI 935,我通过线束连接到936开发板,然后通过mipi接口接到s32v,请问硬件连接之后我在i2c总线上能发现几个设备地址?
我现在只能发现一个936的i2c设备地址0x30,是需要对936进行相应配置才能看到935和相机的地址吗?还是我的硬件板有问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的相机采用AR0144,它的内部集成TI 935,我通过线束连接到936开发板,然后通过mipi接口接到s32v,请问硬件连接之后我在i2c总线上能发现几个设备地址?
我现在只能发现一个936的i2c设备地址0x30,是需要对936进行相应配置才能看到935和相机的地址吗?还是我的硬件板有问题?
和主机直接相连的slave是936 ,所以直接可以通信的就是主机和936.
对于935 和相机来说,都属于remote SER和remote slave,需要进行配置才能找到相应的地址。
建议参考这篇应用手册,针对的是913/914,但方法是一样的: