您好,我在用LMX2571产生4FSK调制的信号的时候,写入寄存器检查多遍是正确的,但是出来的FSK频率不对,频偏+-10khz是正确的,但是20khz按照数据手册相应公式写到寄存器出来的频偏是+-2khz,FSK功能使用的是LMX2571的PIN Mode模式,如图1,载频设置为180Mhz,频偏设置为+-10Khz和+-20khz,而出来的波形频率为150多Mhz,在数据手册上有一处不太理解,FSK功能是N分频器的分数部分分母DEN必须为0,难道是因为对一个频率使用FSK功能后频率会发生改变?