This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595 RAMP功能使用问题

Other Parts Discussed in Thread: LMX2595EVM

试用LMX2595EVM时候,想要产生一个频率递增的LFM信号,8G-8.05G,TICS PRO设置如下

产生的频谱如下:

如果将RAMP0的next_ramp设置为RAMP1,则频谱正常,如下图

请问是哪里出了问题呢?

  • 您好,您的问题正在确认中,如有答复,会立即通知您。
  • 您好,您的问题我已经在英文 E2E上咨询了美国那边的工程师,请参考他的回复,给出了三种ramp 的方式,您看下哪种是符合您的应用需求? 

    然后再进一步讨论:e2e.ti.com/.../829026

    (1) Continuous triangular wave: 8000MHz --ramp up--> 8050MHz --ramp down--> 800MHz --ramp up--> 8050MHz ............

    (2) Repeated triangular wave: 8000MHz --ramp up--> 8050MHz; 8000MHz --ramp up--> 8050MHz; 8000MHz --ramp up--> 8050MHz; ........

    (3) Single ramp: 8000MHz --ramp up--> 8050MHz (stay at 8050MHz)