This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5805



dear 

     图片是我用TAS5805做BTL模式其中的一个通道的负载,(两个4欧姆的喇叭并联然后再串联两个并联的喇叭)当我输入电压到20V电流到1A以上的时候我的TAS5805就会断开,请问是什么原因?

  • 您好, 两个4ohm并联再串联,相当于还是4ohm阻抗。
    datasheet中给出了当PVDD的电压范围再(16V<PVDD≤24V)的时候,负载阻抗最小为4.8ohm。
    当再4.5V≤PVDD≤16V的时候,负载阻抗最小为3.2ohm,所以您可以适当减小工作电压再验证是否还有问题?