This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB933-Q1 PCLK时钟配置

背景:设计了一款摄像头,方案是Sensor+ ISP + SERDES(933),晶振放在ISP上,933的时钟PCLK由ISP提供;

不良现象:通过933对摄像头进行固件烧写或者升级,会出现烧写不了。

                  如果Flash是空白的无参数情况下,ISP无PCLK输出,这个时候会出现914的LOCK信号不稳定,烧写失败;有PCLK了,LOCK信号就稳定了(同一硬件测试结果);

                 FLASH有参数,但是进行升级了,把FLASH中的内容擦除掉后,ISP无PCLK输出,也会出现914的LOCK信号不稳定,升级不成功;(如附件波形);

问题:1、为什么会出现上述现象;

            2、933稳定通信是否一定PCLK?