TUSB211为什么输入输出短接,正常理解信号是往阻抗小的地方通过,如果输入输出短接了,就相当于没有用到TUSB211,那芯片怎么起到信号增强作用????
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TUSB211为什么输入输出短接,正常理解信号是往阻抗小的地方通过,如果输入输出短接了,就相当于没有用到TUSB211,那芯片怎么起到信号增强作用????
您好,您是指的哪里输入输出直接短接?是TUSB211 的框图吗?
看下7.2 Functional Block Diagram 的功能架构,可以看到输入输出之间有高速补偿电路,也就是对信号起到增强均衡作用的电路。
您好,datasheet中这里指的短接,我理解的是D1P和D2P需要连接,而不是D1P和D2M连接,或者说输入输出的极性要保持一致。
因为实际layout时候,差分信号的极性需要对调,这是没问题的,只要保证TUSB211的输入输出极性一致即可。
事实上D1P和D2P之间是有高速信号补偿电路的,在TUSB211的内部架构中也有呈现。
嗯,就是D1P和D2P连接,如果连接了,信号直接从D1P通过外部连线到D2P,没有经过内部的高度信号补偿,那怎么补偿??不太懂
我理解的内部构架是从D1P到内部的高速信号补偿电路,最后D2P输出,这样才能起到高速信号补偿,如果外部连接了,那信号不就不会通过内部的补偿电路了?
您好,D1P是需要经过内部高速补偿电路到D2P的,而不是外部短接,外部短接的话相当于一个buffer,而没起到均衡作用,数据手册中也是指的内部,我理解的就是防止极性发生改变,所以注意是D1P和D2P连接, D1M和D2P连接。
嗯,但是datasheet里面第8页里讲到D1P和D2P必须连接,D1M和D2M必须连接,P12页PCB封装里也显示 D1P和D2P连接,这样的话就不会经过内部的高速补偿电路。所以现在想知道在绘制原理图的时候,D1P和D2P的网络名称是否一样?
您好,看了下TUSB211 的EVM user‘s guide中的电路,确实和datasheet page8中的一样,D1P和D2P, D1M 和D2M 在TUSB211的外部也短接了起来,这样的话,按照以往绘制电路,net name是一样的。
关于这个问题,我看了下,在英文e上也有不少客户咨询这个问题,可以参考下美国工程师的回复:
也就是说,这样物理连接并不是bypass TUSB211, 另外也是为了提高信号完整性,这样的话我认为net name还是要分开:
The connection conducts the signal and when TUSB211 detects USB2.0 HS signal on these lines it will inject current in order to increase the slew rate and by that improve the signal quality of the HS eye diagram.
如果您还有什么问题,请再讨论。